imx8mq evk mfg fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq evk mfg fails

921 Views
deltacluse504
Contributor I

I have trouble with this.

My board's options are 0010 (for eMMC boot) and 01 (for serial download mode)

 

I connected board to my window by usb connector.

 

This is "mfgtool2-yocto-mx8-evk-emmc1.vbs" in mfgtools-with-rootfs folder.

I don't know why this cannot find my board and drive.
I didn't edit "UICfg.ini" and "cfg.ini."

 pastedImage_2.png

 

 

< Device Manager >

pastedImage_5.png 

 

< HyperTerminal Connection >

pastedImage_1.png

< MfgTool.log >

DLL version: 2.7.0
Thursday, July 26, 2018 18:27:06 Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: DeviceTypeDisk--_devices size: 2
ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:3, Volume->_diskNumber:2
ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:2, Volume->_diskNumber:2
ModuleID[2] LevelID[10]: DeviceTypeDisk--find Disk device: 00C67DB0
ModuleID[2] LevelID[10]: DeviceTypeDisk--_devices size: 2
ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:3, Volume->_diskNumber:3
ModuleID[2] LevelID[10]: DeviceTypeDisk--find Disk device: 00C543D8
ModuleID[2] LevelID[10]: Device::hubIndex::getmsc, return the port index is: 10
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop

ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed
ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed
ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - EVENT_KILL
ModuleID[2] LevelID[10]: CMyExceptionHandler::OnMsgExceptionEvent() - KillExceptionHandlerThread
ModuleID[2] LevelID[10]: Exception Handler thread is closed
ModuleID[2] LevelID[1]: delete MxHidDeviceClass
ModuleID[2] LevelID[10]: Device Manager thread is closed

Tags (4)
0 Kudos
3 Replies

664 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sehan

please check that correct (usb otg, usb cable type C to PC) port was used and set

EVK in Serial Download mode using switch settings, look at MX 8M EVK Board Hardware User's Guide

https://www.nxp.com/docs/en/user-guide/IMX8MDQLQEVKHUG.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

664 Views
deltacluse504
Contributor I

Should I use usb otg or C type?

from board to laptop?

I checked Serial Download mode.

Or.. is there other steps before connect this?

I didn't do anything after I bought this.

Just install driver for this connection from here(Virtual COM Port Drivers )

pastedImage_2.pngpastedImage_1.png

0 Kudos

664 Views
igorpadykov
NXP Employee
NXP Employee

please check video Getting Started with the i.MX 8M Evaluation Kit

Getting Started with the i.MX 8M Evaluation Kit|NXP 

Best regards
igor

0 Kudos