Hello,
I have question about CAN-FD example MPC5748G-FlexCAN_FD-TX_RX-test-GHS614.
When I try to execute it the CAN_0 and CAN_1 initialization performed OK, but when I try to send message
over the bus the send sequence stops always on the flags check line.
The question is:
Is somebody have the same problem and can help me to solve the problem..
For information I use the following:
MCU: SPC5748GGMMJ6 1N81M on the Demo Board.
Header file: from example, because my original header file MPC5748G_4.0.01_1N81M.h, but it not contain
information about CAN-FD settings EDL, BRS, ESI.