Hello,
I see that there is flexbuild for LSDK v18.06, when there will be Yocto QorIQ SDK v2.0-1806 (for LS2088ardb)?
I have manually updated Yocto SDK 17.12 which can be downloaded from GitHub - qoriq-open-source/yocto-sdk .
NXP offers Linux SDK 2.0-1703 BSP for the LS2088ARDB board.
See SDK 2.0-1703 documentation:
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
NXP offers also new Linux BSPO for ARM base processors - LSDK.
This LSDK supports the LS2088ARDB board.
See LSDK documentation:
https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.06.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, NXP offers Linux SDK 2.0-1703 but when it gets current update?