Do IMX8M Quad EVK Board has support for WM8960 Codec Driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do IMX8M Quad EVK Board has support for WM8960 Codec Driver?

805 Views
prasanna_mrh
Contributor I

Do IMX8M Quad EVK Board has support for WM8960 Codec Driver?

0 Kudos
1 Reply

646 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can see the schematic of the IMX8M Quad EVK Board, the default design is WM8524 in the board. You can see the schematic for the details. About the audio driver you can see files are under sound/soc in source code. The WM8960 are default design for i.MX6&i.MX7. Hope this can do help for you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos