AnsweredAssumed Answered

JN5168 Error: Unknown Endpoint

Question asked by dogboy21 on Jul 23, 2018
Latest reply on Jul 28, 2018 by dogboy21

Hello,

 

I'm currently trying to create an application for my JN5168 MCU, based on the JN-AN-1171 application note.

When I want to connect it to my Hue Bridge, the log shows that the MCU joined the Zigbee network as a router as expected. However after that, the error E_ZCL_ERR_EP_UNKNOWN shows up for every endpoint configured in my app.zpscfg. The error is triggered by command 0x0A, which seems to be the "Report Attributes" command. I correctly register the endpoints in the application with eZLL_RegisterColourLightEndPoint and also double checked with debug outputs. The tsZCL_EndPointDefinition of the device is also correctly populated with all properties, so I don't quite understand the cause of the problem.

 

Maybe someone knows an answer.

Thanks in advance!

Outcomes