AnsweredAssumed Answered

How to enable KW41Z BLE Examples semihost debug console?

Question asked by Ashish Patel on Jul 23, 2018

Hi,

 

There is setup of KW41Z based BLE SDK on MCUXPresso IDE.

How could I enable the semihost debug console for ble examples?

 

The few examples are imported into IDE but when I check "quick setting" > "SDK Debug Console" > there are two options "Semihost Console" and "UART Console" and both are disabled and also "quick setting" > "Set library/header type" > options are also disabled. How should I enable all the options and run any project debug console? 

Please find the attached the images for the above cases.

 

KW41Z Firmware Details

  • SDK version - 2.2.0
  • Manifest version - 3.0.0
  • Library -  _ble_4-2_host_peripheral_cm0p , _ble_kw41z_controller

Preprocessor

  • SDK_DEBUGCONSOLE=1
  • CR_INTEGER_PRINTF
  • DEBUG
  • And more which are required

I have followed the post of this community before creating the examples in IDE.

"Implement debug output to ble example frdm-kw41z "

So please provide the solution as soon as possible.

Thanks in advance.

 

Regards,

Ashish

Attachments

Outcomes