AnsweredAssumed Answered

Can you produce different voltage frequencies out of different channels of the same instance of the FlexTimer module ?

Question asked by Barak Avigdory on Jul 23, 2018

Greetings,

       I am trying to produce two different frequencies of square waves as a PWM output, the problem is that the two devices I work with are connected to the same FTM instance via different channels.

 

After studying the module registers and using the debugger to inspect them directly, it seems like there is no such option (I can use more than one source clock).

 

Am I correct? Is there an option I haven't considered?

 

thanks ,

             Barak.

Outcomes