AnsweredAssumed Answered

Newbish question on Timer module and valid time settings.

Question asked by Thomas Ekstrom on Nov 18, 2008
Latest reply on Nov 26, 2008 by Jack Skidanov
Hi. This is a pretty dumb question I'm sure, but still, if there is an easy way to solve this, please help...

I am involved in making a project for a HC12 and I use TI1 TimerInt bean. This is currently set to an interrupt period of 256us. Now, this baby is supposed to pulse at, say, 10Hz, so obviously I'd be very, very happy if I could somehow set the period to 250us or 1ms, exactly. However these values are not valid due to clock frequency. Is there an easy way to do this?

Happy for any help,

Kindly, Thomas

Outcomes