SGTL5000: only one DAP available??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000: only one DAP available??

530 Views
our
Contributor I

Do I understand right that I should choose where to use the single available DAP:

in ADC ---> I2S path

or in I2S ---> DAC path?

Isn't it a strange approach?

0 Kudos
2 Replies

470 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alex

one can look at programming steps in sect.2.2.3 Input/Output Routing

AN3663 SGTL5000 Initialization and Programming

http://cache.freescale.com/files/analog/doc/app_note/AN3663.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

470 Views
our
Contributor I

Igor,

During the last work night I already ended up with working design, so I am not at the beginning.

Now I use DAP in the path of I2S ---> DAC,

but in the path of ADC ---> I2S I also need some filtering, but I cannot see the second DAP.

So I want to know definitely:

1) Genious designers of the IC are sure that everybody need filtering only in one path (actually, almost everybody need both).

2) I am so stupid that I can not find the second DAP (at least a few biquads for a IIR filter).

0 Kudos