i.MX6UL RS485 direction control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL RS485 direction control

Jump to solution
1,488 Views
felixhsu
Contributor III

Hi All 

The reference manual mention as below spec. 

RS485.JPG

Could you tell me the direction control via CTS_B pin is hardware auto switch or software handle switch?

Thanks.

Labels (4)
1 Solution
1,226 Views
linda_zhang
Contributor IV

Yes, Felix. Through software control. 

View solution in original post

0 Kudos
4 Replies
1,226 Views
igorpadykov
NXP Employee
NXP Employee

Hi Felix

seems it is hardware as descrbed in sect.53.7.1 Generalities, Figure 53-12. RS-485 driver connection

i.MX6ULL Reference Manual :

The CTS_B pin can be used to control RS-485 output driver outside the chip.

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,227 Views
linda_zhang
Contributor IV

Yes, Felix. Through software control. 

0 Kudos
1,226 Views
linda_zhang
Contributor IV

We are using RS-485 driver direction control via gpio on MYIR MYS-6ULX board.

Through CTS_B might be also possible. 

But for any ways, you need to configure dts.

1,226 Views
felixhsu
Contributor III

Hi Linda

Thank for your reply.

So direction control is software control, right?

it is not hardware will auto detect switch timing. 

0 Kudos