I want write some value to fuse
In uboot I try "fuse prog 3 0 xxxx"
And then I use "fuse read 3 0", out put 0
It seem the command did not take effect
Before I need to use "fuse prog 3 0" , Any pre-operation such as the need to do other bits to be rewritten?
Hi 浩 刘
fuses may be locked, please check Table Lock Fuses in Chapter
Fusemap Reference Manual processor which are you using.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------