AnsweredAssumed Answered

iMX7Sabre board 'PingPong' demo

Question asked by Manuel Kreutz on Jul 17, 2018
Latest reply on Aug 15, 2018 by Manuel Kreutz

Hello,

 

I'm stuck in getting the demo "PingPong" running on the iMX 7 Dual Sabre board REV D.

 

Settings:

- Software Packs installed and used for device "MCIMX7D7"

- uVision 5 as IDE with KEIL ULINK/ME as debugging device for the M4

- Linker and Target options set as shown in files "uVision_Target.jpeg" and "uVision_Linker.jpeg"

- SD card with pre-installed Linux distribution from NXP

 

Steps:

1. Stop Linux doing autoboot

2. Start debugging the demo in uVision

3. Demo on the M4 is initialized correctly I guess -> output shown in "SerialMonitor_M4.jpeg"

4. After starting Linux with command "boot" -> the initialization is stuck within the "starting kernel ..." operation (file "SerialMonitor_A7.jpeg") and wouldn't continue to get Linux running to check the communication between the processors (without debugging the demo it is possible to run Linux without any problems)

 

Did I forget something to set or change in the settings?

I have no idea how to solve that problem and will appreciate any tip or hint...

 

Thanks in advance and best regards,

Manu

Outcomes