Help With MCIMX6QPAICPU3 - i.MX 6 Quad Plus SABRE Automotive Platform CPU Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help With MCIMX6QPAICPU3 - i.MX 6 Quad Plus SABRE Automotive Platform CPU Card

422 Views
mauricedidio
Contributor I

Hi guys,

I hope there is someone that can help me with an digital cockpit integration on a classic car.

Hi have all the TFT screens and MCIMX6QPAICPU3 - i.MX 6 Quad Plus  SABRE Automotive Platform CPU Card.

I do understand that more hardware is needed, but would like to work closely with an experienced operator to help me put this all together.

I am based in Melbourne Australia, if their is someone near me would be preferable but not necessary.

I hope to hear from someone soon,  even if it is to recommend someone.

Here is a link of what I would like to accomplish.

https://www.youtube.com/watch?v=KrCPQ55m_RM <https://www.youtube.com/watch?v=KrCPQ55m_RM

Thank you

Labels (1)
0 Kudos
1 Reply

334 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maurice

one can look at documentation on that board

SABRE|Automotive-Infotainment|i.MX6|NXP 

Schematics (5)
Design files for i.MX 6QuadPlus CPU3 Card with AVB

SABRE|Automotive-Infotainment|i.MX6|NXP 

As mentioned on p.17 schematic parallel display is compatible
7" 800 x 480 LCD and software driver available from Boundary Devices.

Configuring i.MX6 boards for different screens - Boundary Devices 

Other lcds are supported in NXP BSPs described on

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos