Angelo Bertuletti

Fault on backlight circuit of MIMXRT1050-EVK

Discussion created by Angelo Bertuletti on Jul 13, 2018
Latest reply on Jul 27, 2018 by Carlos_Musich

I have done some climatic test using the dev-board MIMXRT1050-EVK.
After few hours I have stopped because I my TFT was off.
I have found U8 (UM1661) hot and C88 (4.7 uH, 6.3 V) in shortcircuit.
The rated voltage of the capacitor is not enough to be used for the backlight circuit, it's required at least a 25 V.

Outcomes