MPC5777C JTAG minimum signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C JTAG minimum signals

Jump to solution
2,318 Views
EAlepins
Contributor V

What is the minimum JTAG signals that should be routed to my JTAG connector for the MPC5777C debugging to work properly?

Thanks.

Étienne

Labels (1)
Tags (2)
0 Kudos
1 Solution
1,945 Views
randyd
NXP Employee
NXP Employee

TDI, TDO, TMS, TCK, RESET, JTAG Supply voltage reference (VREF), and ground.

JCOMP depends on the debugger that you are using. Some debuggers allow the JCOMP to be pull high on the board and not connected to the JTAG connector. They include a command to override the debugger having to drive the signal. However, some debugger do not include this functionality. You should check with your debugger supplier. 

RDY and EVTI are optional signals. RDY allows for faster block moves over the JTAG interface. This can be beneficial during flash programming. 

See the MPC5777C Hardware requirements application note:

https://www.nxp.com/docs/en/application-note/AN5268.pdf 

View solution in original post

0 Kudos
2 Replies
1,946 Views
randyd
NXP Employee
NXP Employee

TDI, TDO, TMS, TCK, RESET, JTAG Supply voltage reference (VREF), and ground.

JCOMP depends on the debugger that you are using. Some debuggers allow the JCOMP to be pull high on the board and not connected to the JTAG connector. They include a command to override the debugger having to drive the signal. However, some debugger do not include this functionality. You should check with your debugger supplier. 

RDY and EVTI are optional signals. RDY allows for faster block moves over the JTAG interface. This can be beneficial during flash programming. 

See the MPC5777C Hardware requirements application note:

https://www.nxp.com/docs/en/application-note/AN5268.pdf 

0 Kudos
1,945 Views
EAlepins
Contributor V

Please answer...

0 Kudos