AnsweredAssumed Answered

S32DS for vision v2.0 build error(import sdk from vsdk)

Question asked by huang tianxiang on Jul 12, 2018

Hi,

      It's my first-time use S32DS for vision, I refer the Release note:

I have copied the SDK folder to S32ds install folder.

However, when I import the sample project(e.g. isp_sonyimx224_csi_dcu) and build it, there are 2 problems I can't fix. 

The first problem is the OSDIR is not defined.

After I modified the OSDIR to "linux" there is a new problem.

 

Is there anyone has the same problem, Thanks.

My PC environment is:

Win10_64bit

S32DS for vision newest one.

Outcomes