AnsweredAssumed Answered

PN7150 or CLRC663?

Question asked by Kevin Timmerman on Jul 12, 2018
Latest reply on Jul 16, 2018 by Kevin Timmerman

Hi, I'm designing an access control product that needs to support all MIFARE and ISO 15693 cards. I am already using an ARM Cortex-M3 part for some other features of the product and need to decide between using the CLRC663plus and the PN7150. It seems like the PN7150 is a no-brainer since it has all the library firmware already included thus saving on my MCU's flash, RAM and processing as well. Is there any disadvantage to using the PN7150 instead of the CLRC part that I'm not seeing? Even the pricing is better on the PN7150.

 

Thanks!

Outcomes