Hello. I am really new to codewarrior and freescale.
I just get some source code from somebody for study.
CPU model is S12XDP512, and Project was made by IDE V 4.5
Now I am using IDE V 4.7.1
When I open that project file(*.mcp), I just get two errors from errow window.
First error massege is below..
-------------------------------------------------------------------------------------------------------------
CPU
|_!ERROR: ERROR int the bean setting. More details provided by Bean inspector
for this bean.
So, I double-click it, then go to bean inspector for CPU below.
MEMORY MODEL BANKED
!GENERATE PRM FILE yes
STACK specification SIZE
STACK SIZE 0080
!Memory segments
Set default memory segments Click to set default
!ROM/RAM segments 34 +-
!Segment0 Enabled EEPROM
Name EEPROM Value(unique identifier)is duplicated
with another module in project
Qualifier NO_INIT Warning: This segment is not used
by default. It is necessary to
specify user placement manually.
---------------------------------------------------------------------------------------------------------------
----------------------------------------------------------------------------------------------------------------
Second one is below
! EEPROM
|_ERROR: Erro in the bean settin. More details........
So, I double-click it, the go to Bean Inspector EEprom:IntEEPROM
Bean name EEprom
EEPROM intEEPROM IntEEPROM
Interrup service/event Disabled
!Address range
!Start address 0 There is I/O Space from 0x0000 to 0x07FF, but
required memory is internal EEPROM.
!Used size 0 Set correct size of the EEPROM array. The bean
inspector expected non-zero size of the used array.
Used exclusively yes
!Page size 400 Maximum value available in actual bean setting
is only 0 Bytes.
--------------------------------------------------------------------------------------------------------------
Something is wrong on banked memory setting on CPU bean, and intEEPROM bean.
I could not find out. Please some one help me out to complie and debug it on my
Codewarrior.
Regards..