I was looking at the USB examples from the SDK of the LPCXpresso5411. Using the example "SDK_2.2.1_LPCXpresso54114/boards/lpcxpresso54114/usb_examples/usb_rom_device_msc_ram" I successfully got a PC to recognise the LPCXpresso5411 as a USB device with a USB cable using the hard coded files in ramdisk.c. eg the code below will show basic files when a usb cable is plugged into a PC.
//ramdisk.c
static const struct FAT12_img
{
const uint8_t *data;
int offset;
int size;
} FAT12_img[] = {
/* Each sector is of size 512 Bytes i.e., 0x200 Bytes */
{FAT12_header, 0, sizeof(FAT12_header)}, /* FAT12 at sector 0,1 */
{FAT12_root_dir, 0x400, sizeof(FAT12_root_dir)}, /* Root dir at sector 2 */
{FAT12_file_readme_txt, 0x600, sizeof(FAT12_file_readme_txt)}, /* README.TXT file data */
{FAT12_file_index_htm, 0xC00, sizeof(FAT12_file_index_htm)}, /* INDEX.HTM file data */
};
void DataRam_Initialize(void)
{
int i;
extern uint8_t g_memDiskArea[];
memset(g_memDiskArea, 0, MSC_MEM_DISK_SIZE);
for (i = 0; i < sizeof(FAT12_img) / sizeof(FAT12_img[0]); i++)
memcpy(&g_memDiskArea[FAT12_img[i].offset], FAT12_img[i].data, FAT12_img[i].size);
}
However I would like to integrate this with the FatFs for an SD card. With help from this forum, I have the FatFs and SD card working. So instead of the "static struct FAT12_img" I m trying to use the FIL structure from ff.h.
//ff.h
typedef struct {
_FDID obj; /* Object identifier (must be the 1st member to detect invalid object pointer) */
BYTE flag; /* File status flags */
BYTE err; /* Abort flag (error code) */
FSIZE_t fptr; /* File read/write pointer (Zeroed on file open) */
DWORD clust; /* Current cluster of fpter (invalid when fprt is 0) */
DWORD sect; /* Sector number appearing in buf[] (0:invalid) */
#if !_FS_READONLY
DWORD dir_sect; /* Sector number containing the directory entry */
BYTE* dir_ptr; /* Pointer to the directory entry in the win[] */
#endif
#if _USE_FASTSEEK
DWORD* cltbl; /* Pointer to the cluster link map table (nulled on open, set by application) */
#endif
#if !_FS_TINY
BYTE buf[_MAX_SS]; /* File private data read/write window */
#endif
} FIL;
Would I do something like
FIL fil;
memcpy(&g_memDiskArea[fil.obj], fil.buff, fil[i].size);
I m not too sure how to do this, but any point in the right direction would be great.
Thanks,
Ronan
Hi Ronan,
See you again, yes, I help you finished the SD card detect code with fatfs in LPC54114 last month.
But, associated with the USB, we really don't have any example for your reference now. This is really complicated, you also need to familiar with the USB MSD function.
You can try to modify the USB MSC code, change the usb received data interface which is stored in the internal flash and RAM to the SD card.
This post maybe useful to you, you can check it:
How to add SD card support (SPI) to usb composite msc cdc example?
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------