AnsweredAssumed Answered

Issue with booting PN7462AU from flash

Question asked by gokul krishna on Jul 12, 2018
Latest reply on Jul 18, 2018 by gokul krishna

Unable to boot the PN7462AU after loading the flash with PN7462AU_ex_phExRfPoll release image. I am able to read the card details when the same code is run using in debug mode.

After debugging I am able to note that the control is not returning to the program after executing rf related API's. RF field enable API is not returning to the program. As mentioned previously the same image is used for running the code in debug mode and for flashing the image.Also note that the API is not returning an error value but is not returning to the program.

 

pn7462au help urgent high_priority 

Outcomes