Hi,
I am working on ls1021a based board ( 4.1.8 kernel is running), On the target board i am trying to do soft reboot. Once the reboot command is issued on the target it was hanging at this point "reboot failed --System halted".
please find the log below.
Can you please let me know if anyone have an idea on this ?
Log:
# reboot
Stopping SWUpdate: killall: can't kill pid 170: No such process
OK
Stopping 615AController: stopped /usr/bin/a615acontroller (pid 168)
OK
Stopping telnetd: OK
Stopping sshd: OK
Stopping network: ifdown: interface eth0:1 not configured
OK
Unconfigure by strapping: OK
Saving random seed... done.
De-initializing IO: OK
Stopping logging: OK
Inhibiting Watchdog Count for Soft Reset: OK
umount: devtmpfs busy - remounted read-only
umount: can't unmount /: Invalid argument
The system is going down NOW!
Sent SIGTERM to all processes
Sent SIGKILL tokvm: exiting hardware virtualization
reboot: Restarting system
Reboot failed -- System halted
Regards,
praneeth
Look at the following page about possible problem for reboot:
https://stackoverflow.com/questions/46599579/arm-linux-reboot-process
See also attached file. It is reboot.c code for the LS1021a. Find the machine_restart function.
Perhaps 1 second is not enough for your board to restart.
Test your board using "shutdown" command.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------