Hi,
Create new empty project and in Debug Configurations select your .srec file:
Jiri
I want to use PEMICRO debugger to flash the srec file on S32DS.
To other people who do not have a source code, flash using only srec file, pemicro debugger, and S32DS.
Is this possible?
Hi
Thanks to you, I can falsh the binaries.
Best regards,
Byungju.
what hardware did you use to flash the binary file ?
Hi,
you can use PE Micro OpenSDA interface on EVB or any other supported debug probe - Segger J-Link, PE Micro Multilink, Lauterbach...
Jiri
I have the PE Micro, do i need to connect the micro USB cable ? or only the 12 v power ?
Hi Alaa,
If you are using the S32K144 development board, you can provide power either through the micro USB cable or through the 12 V power cable depending on your Jumper Setting for JP107. Once you have power to the device, you connect the 10-pin mini ribbon cable to the Multilink and should see the orange LED appear which means that the Multilink recognizes the target device. You can then proceed to use S32 Design Studio to debug and flash your device. PEmicro also offers a software that can flash the binary file through a GUI application, or autonomously via command line application which can really help in the production stage once all the code development has been finished. Hope this helps!
Steve