Hi,
Where can i find the code which do XIP (Execution In Place) from external SPI flash (Micron), in the SDK there is Download image XIP example, but I need to run code from the external flash in XIP,
Thanks In advance
Avi Makmal
WINBOND
Hello Avi Makmal
Could you please provide more information of which LPC are you using?
Please take a look into the following application note:
Which explains how to modify the header structure of the image in order to run code from the external flash.
Hope it helps!
Victor.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------