AnsweredAssumed Answered

power on without PMIC

Question asked by victor Wang on Jul 9, 2018
Latest reply on Jul 9, 2018 by victor Wang

Hi community,

I'm working on i.MX6 DL sabreSD board without PMIC.

I build image with Android 6 source code.

 

After I read the document "i.MX Linux® Reference Manual" I tried to modify Power Management configuration in menuconfig to disabled it.

These were what I had done.

disabled CONFIG_PM

disabled CONFIG_SUSPEND

disabled PF100 Regulator Driver

disabled Anatop Regulator Driver

 

But after I disabled all this configuration and rebuild image, it showed error to me and said there is something undeclared.

 

I am afraid that it will cause the system cannot reboot normally or it would dead when I starting the kernel.

 

Here are my questions:

  1. Can I use the same image which included power management on the board which have no PMIC?
  2. If can't what can I do ? Did I just need to set all configurations which are related with PMIC to disabled or I have to modify driver to fitch board which have no PMIC?

 

Thanks in Advanced!

Outcomes