Is there no NXP produced bootloader for the MPC5744P like there is for the Kinetis range of processors?
Is there no NXP produced bootloader for the MPC5744P like there is for the Kinetis range of processors?
Hello Mike,
The RAppID BL utility requires first loading a rbf file onto the board (which I guess is the bootloader itself) which is how the utility talks to the MCU to perform the download. This seems to behave as it should for model based design applications, however I cannot get this to work for downloading applications over CAN.
Outlook <https://aka.ms/ghei36> for<https://aka.ms/ghei36> Android<https://aka.ms/ghei36> herunterladen
Von: mikedoidge
Gesendet: Montag, 9. Juli, 22:22
Betreff: Re: - Re: Bootloader for MPC5744P
An: Chulue Zhong
NXP Community
Re: Bootloader for MPC5744P
reply from Mike Doidge in S32 Design Studio - View the full discussion
Hello,
There is RAppID Bootloader . You can download it from RAppID Boot Loader Utility . It is located on the product page for RAppID Initialization for Power Architecture | NXP .
Hope it helps ,
Mike
Reply to this message by replying to this email, or go to the message on NXP Community Start a new discussion in S32 Design Studio by email or at NXP Community Following Re: Bootloader for MPC5744P in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
Hello,
There is RAppID Bootloader. You can download it from RAppID Boot Loader Utility. It is located on the product page for RAppID Initialization for Power Architecture|NXP.
Hope it helps,
Mike