AnsweredAssumed Answered

imx8mqevk, mfgtool QSPI configuration

Question asked by Jeff Kim on Jul 4, 2018
Latest reply on Jul 5, 2018 by igorpadykov

Hello,

 

I'm trying to burn u-boot image on QSPI by mfgtool. I chose mfgtools-with-rootfs-mx8 package.

From u-boot log on screen, I saw the QSPI is n25q256a of STMicro.

In cfg.ini file, "name = SDCard" was the default configuration. It seems to be modified.

I saw two Nor Flash names from ucl2.xml. They are "Quad Nor Flash" and "FlexSPI Nor Flash".

"Quad Nor Flash" has u-boot files for MX6 and MX7 only according to ucl2.xml.

Do I have to choose name="FlexSPI Nor Flash" for MX8QM device?

If so, eventually imx-boot-imx8qmlpddr4arm2-sd.bin-flash_dcd will be used. Is it suitable for QSPI n25q256a?

 

Regards,

Jeff

Outcomes