i.MX6 Quad/Dual chip force limit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Quad/Dual chip force limit

454 Views
andychien
Contributor III

Dear Sir,

Customer ask about chip force limit  on the i.MX6 Quad/Dual die itself when the heat-sink/thermal pad is torqued down?

 I found NXP AN4871 documents about Assembly Handling and Thermal Solutions for Lidless FCBGA.

i.MX6 Dual/Quad are 21x21mm package, but below table 5 doesn’t have 21x21mm body size info.

Could you help check and provide it?

Thanks a lot,

snap.jpgdoesn’t have 21x21mm body size info.

Labels (2)
0 Kudos
1 Reply

387 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

below recommendation from app team:

"NXP recommends that the maximum load force not exceed 10 lbs, particularly for unlidded devices."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos