AnsweredAssumed Answered

MCUXpresso IDE and CMSIS DSP

Question asked by Jason William on Jul 2, 2018
Latest reply on Jul 8, 2018 by Alice_Yang

1. Hello, I use MCUXpresso IDE v10.2.0, I am now developing a two - way audio signal real-time collection and processing of the project, which use the CMSIS-DSP software library. I haven't used this IDE before. So, as long as I create a new project, it contains DSP and doesn't need me to add it in the CMSIS file. Is that right?

 

2., and where can the driver API function be used to find their HTML file descriptions? I want to see the function and the meaning of the parameter.

 

3. after joining the ADDA demo, save the following problems: no such file or directory, how do I solve it?

 

4. how to quickly master the programming method of MCUXpresso IDE v10.2.0? I had previously learned the SDK programming of Xilinx FPGA.

 

Thank you very much, Jason

Outcomes