AnsweredAssumed Answered

Where to find LPCXpresso1549 SDK for MCUXpresso?

Question asked by seneryetgin on Jun 28, 2018
Latest reply on Jul 1, 2018 by ZhangJennie

Dear all,

 

I am excited to have board LPCXpresso1549. I can be considered beginner so please bear with me.

 

I have installed MCUXpresso. I could create a project (C/C++ project), I can even flash the default code using IDE, so far so good. After I confirmed the board is ready to go, now I am willing go further and try some sample codes.

 

But, I noticed that I don't have any SDK installed. And while creating a project, I don't see IMPORT button although the user manual mention about it. I think, the version I have is not supposed to do so, not sure.

(I have this version: MCUXpresso IDE v10.2.0 [Build 759] [2018-05-15] )

 

And I found a place supposed to make one for me (https://mcuxpresso.nxp.com/en/select )

But, no avail. Because, my board is not mentioned.

 

So, what am I missing?

Do I choose a wrong project type?

Don't I have any SDK pre-installed or so?

The board I have is not supported by MCUXpresso?

 

Note that: For me, I like to use low level libraries as much as possible in order to learn some inner workings.

 

Thanks a lot for your inputs from now.

 

Regards,

Sener

Outcomes