LCD BLANK SCREEN AFTER WAKEUP WITH POWER KEY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD BLANK SCREEN AFTER WAKEUP WITH POWER KEY

486 Views
himabindu
Contributor III

Hi Team,

                Iam working on Power Management for IMX6SL Board(ARM Architecture).Using the  command

echo mem >/sys/power/state i am entering into the suspend state. With the help of gpio_to_irq  for Watchdog reset pin and Power Key, using IRQ_EARLY_RESUME flag I am successfully able to wakeup the device.But only issue is that I am unable to get the previously stored Gnome desktop.Also Iam unable to get any image on the framebuffer when cat image on to Framebuffer.Kindly provide me any solution for the same.

Thanks & Regards,

C.Himabindu.

Labels (1)
0 Kudos
1 Reply

417 Views
igorpadykov
NXP Employee
NXP Employee

Hi HIMA

what bsp used in the case, may be useful to check

ubuntu boundary devices releases, for BD-SL-i.MX6 board

https://boundarydevices.com/trusty-ubuntu-mx6/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos