i installed the CodeWarrior for 68k V 3.3.1 / 4.2.7 , but i think this is to new for my old CPUs, i can't find this CPUTypes as target.
i need one that supports the 68020 and 68030 CPU, there are a older Version available that supports this?
i would like to build a hardware monitor with mc68901 DUART Controller, there are possibly libs avaible in a archive?
best regards, jan
Hi
These two devices 68020 and 68030 have been discontinued since around 18 years ago. We are short of support these devices for both HW and SW.
I suggest you use 3rd party IDE if in need. for example
https://www.ghs.com/products/68k_development.html
http://www.cosmic-software.com/68k.php
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------