running uMTP responder hangs iMX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

running uMTP responder hangs iMX6ULL

1,046 Views
priteshpatel
Contributor I

Hi,

I have been trying to add MTP support in iMX6ULL. Linux kernel version is 4.1.15.

I found open source uMTP responder online.

GitHub - viveris/uMTP-Responder: Ligthweight Media Transfer Protocol (MTP) responder daemon for GNU/... 

It is a user space MTP daemon written in "C".  It runs through gadgetfs. You can find more information and source code  in above link.

I have followed below steps to run it on iMX6ULL EVK.

modprobe gadgetfs

mkdir -p /dev/gadget

mount -t gadgetfs none /dev/gadget

When I run the mtp daemon, EVK got hanged. I could no longer operate EVK on serial console. The host PC which is connected to EVK through OTG can not read USB descriptor information. USB device could not be enumerated in host PC.

Below are the debug logs.

root@imx6ull14x14evk:~/uMTP-Responder# ./umtprd
[Info] uMTP Responder
[Info] Version: v0.8.1 compiled the Jun 19 2018@15:21:51
[Info] (c) 2018 Viveris Technologies

[ 23.891322] gadgetfs: bound to 2184000.usb driver

[Debug] init_mtp_responder

[Debug] init_mtp_responder : Ok !

[Info] Add storage home folder - Root Path: /home
[Debug] mtp_add_storage : /home

[Debug] mtp_add_storage : Storage 00000001 mapped to /home (home folder)

[Info] USB Device path : /dev/gadget/2184000.usb
[Info] USB In End point path : /dev/gadget/ep1in
[Info] USB Out End point path : /dev/gadget/ep2out
[Info] USB Event End point path : /dev/gadget/ep3in
[Info] USB Max packet size : 0x200 bytes
[Info] Manufacturer string : Viveris Technologies
[Info] Product string : The Viveris Product !
[Info] Serial string : 01234567
[Info] Interface string : MTP
[Info] USB Vendor ID : 0x1D6B
[Info] USB Product ID : 0x0100
[Info] USB class ID : 0x06
[Info] USB subclass ID : 0x01
[Info] USB Protocol ID : 0x01
[Info] USB Device version : 0x3008
[Debug] fill_config_descriptor: (Total Len : 9 + 30 = 39)
[Debug]
09 02 27 00 01 01 05 80 01
[Debug] fill_if_descriptor:

[Debug]
09 04 00 00 03 06 01 01 06
[Debug] fill_ep_descriptor:

[Debug]
07 05 81 02 00 02 00
[Debug] fill_ep_descriptor:

[Debug]
07 05 02 02 00 02 00
[Debug] fill_ep_descriptor:

[Debug]
07 05 83 03 1C 00 06
[Debug] fill_config_descriptor: (Total Len : 9 + 30 = 39)
[Debug]
09 02 27 00 01 01 04 80 01
[Debug] fill_if_descriptor:

[Debug]
09 04 00 00 03 06 01 01 06
[Debug] fill_ep_descriptor:

[Debug]
07 05 81 02 00 02 00
[Debug] fill_ep_descriptor:

[Debug]
07 05 02 02 00 02 00
[Debug] fill_ep_descriptor:

[Debug]
07 05 83 03 1C 00 06
[Debug] fill_dev_descriptor:

[Debug]
12 01 00 00 06 01 01 00 6B 1D 00 01 08 30 01 02
03 01
[Debug] init_usb_mtp_gadget :

[Debug]
00 00 00 00 09 02 27 00 01 01 05 80 01 09 04 00
00 03 06 01 01 06 07 05 81 02 00 02 00 07 05 02
02 00 02 00 07 05 83 03 1C 00 06 09 02 27 00 01
01 04 80 01 09 04 00 00 03 06 01 01 06 07 05 81
02 00 02 00 07 05 02 02 00 02 00 07 05 83 03 1C
00 06 12 01 00 00 06 01 01 00 6B 1D 00 01 08 30
01 02 03 01
[Info] init_usb_mtp_gadget : USB config done
[Debug] handle_ep0 : Entering...
[Debug] 1 event(s)
[Debug] EP0 DISCONNECT
[Debug] 2 event(s)

I tried debugging chipidea UDC and gadgetfs drivers but could not find the root cause.

I have successfully run uMTP on Beagle bone black. Which uses musb-hdrc.

If anyone have any idea about what could be wrong here, please answer asap.

Labels (3)
0 Kudos
2 Replies

680 Views
b36401
NXP Employee
NXP Employee

Please try to use mtp-tools to manage MTP. Possibly gadgetfs produces the issue.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

680 Views
jean-francois_d
Contributor I

Hi,

You can eventually try the new uMTP Responder version, this may solve your issue.

https://github.com/viveris/uMTP-Responder/archive/umtprd-0.8.6.tar.gz 

0 Kudos