i.MX28 usb fatal error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 usb fatal error

887 Views
iuncuim
Contributor I

Hi all!

I have some trouble with USB on imx287. I have a custom board, with two ethernet, usb modem Cinterion EHS5 and mainline kernel 3.18.20.

When I use two ports at the same time, the usb controller very often dies. For example I unplug two ehternet at the same time:

[ 239.117637] 3g-internet: renamed from ppp0
[ 266.671910] fec 800f4000.ethernet eth1: Link is Down
[ 266.677045] br-lan: port 2(eth1) entered disabled state
[ 267.172576] fec 800f0000.ethernet eth0: Link is Down
[ 267.541847] ci_hdrc ci_hdrc.1: fatal error
[ 267.546001] ci_hdrc ci_hdrc.1: HC died; cleaning up
[ 267.551720] usb 1-1: USB disconnect, device number 2
[ 267.557291] cdc_acm 1-1:1.0: failed to set dtr/rts
[ 267.691796] br-lan: port 1(eth0) entered disabled state
[ 267.702052] fec 800f0000.ethernet eth0: MDIO read timeout
[ 267.731662] fec 800f0000.ethernet eth0: MDIO read timeout
[ 268.201667] fec 800f0000.ethernet eth0: MDIO read timeout
[ 268.241661] fec 800f0000.ethernet eth0: MDIO read timeout

I tried with another kernel (4.14.50) and the problem persisted.

What could be the problem?

Labels (2)
0 Kudos
1 Reply

495 Views
igorpadykov
NXP Employee
NXP Employee

Hi iun

one can check if this could be caused by hardware, look at

AN: Issues often met in i.MX28 application

Application note sharing: Issues often met in i.MX28 application 

usb signal margin may be low, so it may loose connection,

one can check usb layout using AN4215 i.MX28 Layout and Design Guidelines

sect.7 USB

https://www.nxp.com/docs/en/application-note/AN4215.pdf 

Also if usb device is powered from i.MX28 side, one can pay attention if power

is sufficient for normal operation of this device and consider external power supply

if necessary.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos