I use the 3-Phase PMSM Motor Control Development Kit with Qorivva MPC5604P MCU and the User interface of NXP you can see ins Screen.PNG.
If I start the program, there is a failure -Missing symbol Definitions- you can see at Variables.PNG.
But it is connected with the board. (Communication.PNG)
Where is the problem and how can I fix it?
(The motor runs if I use the switch up/down or I update the target with the User interface. But there is no change if I vary the input variables)
Hi,
Did you follow quick start guide and compiled and loaded the code to micro?
Do you have correctly set Freemaster files?
regards,
Peter