Hi, im working with the Trustzone on the IMX6QSD board and i wanted to ask id there's a way to use linux as non-secure in the board.Kind regards,
Ailton Lopes
Hello,
customers can try the recent NXP Linux BSP L4.9.88, which supports Optee, but it
is not enabled by default. For how to enable it, see ReadMe.
https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061...
Documentation - OP-TEE
Regards,
Yuri.
pls refer to the topic as below, hope helpful for you
https://community.nxp.com/message/650147
never-displayed