AnsweredAssumed Answered

i2c transactions cause pwm glitches

Question asked by Nick Preiser on Jun 19, 2018
Latest reply on Jun 20, 2018 by Nick Preiser

I am using a MKV11Z64VXX7,  and all the very latest sdk components/libraries.  (as of 6/19/18) 

 

I have the device configured so that the ftms are being used to drive many independent pwm signals. 

 

When I issue a periodic i2c transaction ,  the transaction is successful,  however, I see a glitch on the 

pwm signals. 

 

Wondering if anyone else has see an issue

 

thanks 

Nick P. 

Outcomes