Does the iMX6q Sabre-lite platform support SDIO 3.0 UHS mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the iMX6q Sabre-lite platform support SDIO 3.0 UHS mode

696 Views
pandivijayaraj
Contributor I

IMX6Q Sabre-lite is booted with kernel 4.9.11 for interfacing an SDIO based WIFI cardsupporting SDIO 3.0. It is detecting the WiFI card as Normal high speed SD card. It is not detecting as UHS SDIO 3.0 card. host supplies 50MHz clock to WiFi card.

Does the iMX6q Sabre-lite platform support SDIO 3.0 UHS mode devices?

Is there any changes to be done in dtb file for this requirement? Any patches available?

Regards,

Pandi Vijayaraj

Labels (3)
0 Kudos
2 Replies

546 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Not supported.

0 Kudos

546 Views
gary_bisson
Senior Contributor III

Hi,

No the SabreLite doesn't support SDIO3.0 operations since it requires to switch NVCC_SDx to 1.8V whereas the design fixes it to 3.3V.

Regards,

Gary

0 Kudos