Linux version : Ubuntu 18.04
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m
imx-4.9.88-2.0.0_ga.xml
DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-xwayland
bitbake fsl-image-validation-imx
ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: QA Issue: /lib/firmware/murata/.git/hooks/fsmonitor-watchman.sample contained in package linux-firmware requires /usr/bin/perl, but no providers found in RDEPENDS_linux-firmware? [file-rdeps]
ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.
ERROR: linux-firmware-1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0 do_package_qa: Function failed: do_package_qa
ERROR: Logfile of failure stored in: /home/user/imx-yocto-bsp/build-xwayland/tmp/work/all-poky-linux/linux-firmware/1_0.0+gitAUTOINC+bf04291309_a0026b646c-r0/temp/log.do_package_qa.1061
ERROR: Task (/home/user/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6743 tasks of which 6720 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/user/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux-firmware/linux-firmware_git.bb:do_package_qa
Summary: There was 1 WARNING message shown.
Summary: There were 3 ERROR messages shown, returning a non-zero exit code.
Do I need to modify Linux-firmware_git.bb file for RDEPENDS? If so, how to modify this?
As far as I know, Ubuntu 18.04 is not validated yet for the build. Could it cause above file-rdeps error?
I might have to install another version such as Ubuntu 16.04 if necessary.
Is it possible to complete bitbake with Ubuntu 18.04 by fixing file-rdeps error?
Any comment for this problem will be highly appreciated.
Hello,
You are right - Ubuntu 18.04 is not validated yet for the build.
Nevertheless, please try to perform "repo sync" after "repo init".
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------