Continuous self test / Built In Test for T1042 SoC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Continuous self test / Built In Test for T1042 SoC

500 Views
antoinedurand
Contributor II

Does a Continuous Self Test, Built In Test, monitoring mecanism exist for T1042, which could be run on top of linux Operating System ?

Thanks.

0 Kudos
1 Reply

334 Views
Pavel
NXP Employee
NXP Employee

The T1042 DDR controller has means for automatic memory testing.

Please refer to the QorIQ T1042 Reference Manual, 14.4.59 DDR Memory Test Control Register (DDR_DDR_MTCR) and next sections.

 

See also the Section 1.3.3.1 of the "QCVS SerDes Tool User Guide":

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos