AnsweredAssumed Answered

S32K Encrypted FlexCAN example

Question asked by Bertrand Tay on Jun 13, 2018
Latest reply on Jun 21, 2018 by Alexandru Nan

Hi,

 

I just got the s32k144evb-q100 board, and I'm testing the encrypted flexcan example found in the S32 ARM installation folder.

 

I followed the instructions in the attached file.

 

When I step through and debug, I can see the TX function being called when I press the pushbutton

 

But on the RX board, I'm not receiving any messages and the LED is not toggling.

 

Not sure what I'm doing wrong here. Do I need some special cables to connect the CAN ports? Currently I'm only using 3 wires to connect the CAN_H, CAN_L and Ground. Based on the schematics, think pin3 is not used.

 

Appreciate any help!

 

Thanks.

Attachments

Outcomes