AnsweredAssumed Answered

temperature sensor

Question asked by Ian Benton on Jun 13, 2018
Latest reply on Jun 14, 2018 by Kerry Zhou

A while ago Where's the WRAPEN field? you told me that the WRAPEN field doesn't exist.

So, on page 491 of the LPC15 manual, it says 

"If the WRAPEN field is 0x2 the temperature sensor voltage is also output on the ADCn_0 pin"

In the absence of the WRAPEN field, would I find the temperature sensor voltage on the ADC pin, or not?

And presumably, it would only be there if the relevant bit in PINENABLE was set?

Outcomes