T2080 ECn_GTX_CLK125 Usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 ECn_GTX_CLK125 Usage

Jump to solution
781 Views
2007031026
Contributor II

Hi,

    In my design,I only use the T2080  CPU's SGMII interface for Ethernet,is it necessary to connect the ECn_GTX_CLK125 pin with a 125MHz reference clock?

    Thanks!

Tags (1)
1 Solution
667 Views
alexander_yakov
NXP Employee
NXP Employee

"When operating in SGMII mode, the ECn_GTX_CLK125 clock is not required for this port." - Section 3.19.9.1 of T2080 datasheet.

When this pin is not used, it is recommended to pull this pin low through a 2-10 kΩ resistor to GND (T2080 Design Checklist, Tables 29 and 30) 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
668 Views
alexander_yakov
NXP Employee
NXP Employee

"When operating in SGMII mode, the ECn_GTX_CLK125 clock is not required for this port." - Section 3.19.9.1 of T2080 datasheet.

When this pin is not used, it is recommended to pull this pin low through a 2-10 kΩ resistor to GND (T2080 Design Checklist, Tables 29 and 30) 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

667 Views
2007031026
Contributor II

Thank you!

0 Kudos