AnsweredAssumed Answered

Cannot flash OM13098 or OM13088

Question asked by Amr Abdelrahman on Jun 10, 2018
Latest reply on Jun 11, 2018 by Brendon Slade

Hello All,

 

I bought OM13098 and OM13088 and followed all the instructions to flash the two boards but in vain. I went through all the possible solutions here in the support forum but none of these worked out.

 

I tried with LPCXpresso v8.2.2_650 and MCUXpresso v10.2.0_759 under Windows 10 Home edition 64-bit.

The boards cannot be identified in the device manager under Ports section.

 

Is there anyway to manually install the needed drivers and connect to these boards ?

 

Thanks in advance.

Outcomes