In imx6 oreo sabresd_6dq_car-userdebug work on which NXP board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In imx6 oreo sabresd_6dq_car-userdebug work on which NXP board

385 Views
vivektol
Contributor I

Hi All,

           We have compile imx6 Oreo build with lunch option sabresd_6dq_car-userdebug

Now we have questions that on which NXP development board it will work.

If any idea please reply.

0 Kudos
1 Reply

285 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Vivek Tol,

The sabresd_6dq_car-userdebug profile is defined but it’ not listed on the Release Notes of the BSP as part of the supported images so I would recommend using the sabresd_6dq-XXX images instead. The image should run on the i.MX6 Dual/Quad SABRE SDP, but since it’s not listed it is not supported as sabresd_6dq_car-userdebug.

Regards,

0 Kudos