AnsweredAssumed Answered

RT1050 SDRAM Configuration Issue?

Question asked by Joshua Sakwa on Jun 6, 2018
Latest reply on Jun 6, 2018 by Wigros Sun

I noted a post on another forum that suggests a possible driver defect in SEMC_ConfigureSDRAM(...);

 

The post suggests that line 387 of fsl_semc.c contains a defect. Specifically the post suggests that the refresh timer should be enabled here by ORing in SEMC_SDRAMCR3_REN_MASK -- I noticed that this is done on line 417 in SDK version 2.3.1. Is this a potential issue that I will want to fix locally, or is the Embedded Wizards forum post stale? 

 

Thanks in Advance,

Joshua

Outcomes