AnsweredAssumed Answered

Flash blocks of the CSE

Question asked by Ibrahim Salem on Jun 6, 2018
Latest reply on Jun 18, 2018 by Peter Vlna

I'm currently working on a project that uses S32R274 micro controller.

 

I was reading the CSE section on the data sheet S32R274RM version 3.1. It is mentioned that there are two dedicated flash blocks that are accessible only by the CSE and they are used for storing the command processor firmware and memory slot data. However, I couldn't find any mentioned interface (ex: command) for the CSE to use those memory blocks.

 

Outcomes