AnsweredAssumed Answered

Missing "/dev/fb1" overlay framebuffer device in Linux on the i.MX6Q

Question asked by Miroslav Musil on Jun 7, 2018
Latest reply on Jun 11, 2018 by Frantisek Hacker

Hello,

 

Our team was able to run our developped application on the i.MX6Q SABRE EVK board with Linux system based on the Yocto (Morty) project (with kernel 4.9.11). Our application uses the background framebuffer ("/dev/fb0" device) together with the overlay framebuffer ("/dev/fb1" device) to get desired functionality for graphics.
Our next goal, we are working now, is to create a new Linux based SW platform running Linux kernel 4.14.0 (we use vanilla kernel sources with some our patches, the Yocto project is not involved any more). The new SW platform is running fine on the i.MX6Q SABRE EVK board, but there is only one framebuffer device spawned during the system startup - only the "/dev/fb0" framebuffer device is present, the "/dev/fb1" overlay framebuffer device is missing.

 

What system entity is responsible for spawning the overlay framebuffer device during the system statup ?
What shall we do to get the overlay framebuffer available ?


Thank you in advance.


Best regards

Miroslav Musil

Outcomes