iMX6Q Pinning Parallel Camera 12-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q Pinning Parallel Camera 12-bit

Jump to solution
732 Views
michael_irsfeld
Contributor I

Hello,

I'm trying to interface two cameras (Bayer12) via parallel sensor interface. In datasheet of iMX6Q on table 64 I can only find which IPU ports i should use for a 16-bit camera. Which IPU-Ports should I use for 12-bit camera?

Thanks
Michael

Labels (3)
0 Kudos
1 Solution
539 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi michael,

For possible sensor connections, please look at the datasheet(s),

for example - Table (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC.

https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

IPU0-1 can be used for 12bit.

View solution in original post

0 Kudos
1 Reply
540 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi michael,

For possible sensor connections, please look at the datasheet(s),

for example - Table (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC.

https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

IPU0-1 can be used for 12bit.

0 Kudos