use SSI1 to be I2S, i made a dummy sound card to force output audio, but the audio frequency is not 48kHz, but 49.6kHz. and blck is not 3072kHz, but 3172kHz.
where should i check, please give a advance, thanks.
and i change the ssi_clk parent from "pll3_pfd_508M" to "pll4_audio_main_clk" in arch/arm/mach-mx6/clock.c, got the same result.
Hi 家禄 刘
please refer to Chapter 8 Porting Audio Codecs to a Custom Board
attached Porting Guide, probably parent pll value should be adjusted for
produced accurate audio frequency clock.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------