AnsweredAssumed Answered

How to connect two LPC 1769 boards over a wireless network?

Question asked by Aamir Bader Shah on Jun 2, 2018
Latest reply on Jun 18, 2018 by Carlos_Mendoza

I intend to connect 2 LPC 1769 Boards over a wireless network and then use a TTC schedule architecture to code a basic program (such as a fire alarm system) and then be able to measure the jitter time for the instructions that are exchanged between the two boards. However I need help with the following questions:

 

1. How do I connect 2 LPC Xpresso boards wirelessly? If I need to use Xbee, which module should I use? Is there a guide on this?

 

2. Once connected wirelessly, how would the 2 boards exchange real time information?

 

3. What wireless protocol do I need to follow for the communication between the two boards.

 

4. How can I measure the jitter time of instructions between the 2 boards?

 

5. Any other info, link or resource regarding this project  or a similar tutorial will be helpful. 

 

Thanks.

 

Shah

Outcomes